Eaton Logo

Controls

What is the difference between a vacancy sensor and an occupancy sensor ?

What is the phone number for Cooper Controls ?

Can I get a manual for a Novitas 01-400 occupancy sensor?

What is walk-through mode on a sensor?

Where can I get a Novitas switchpack (part# 13-051)?

Can I block a PIR motion sensor’s view?

OAC-DT Motion Sensor Troubleshooting

Can the Photodiode Sensor (DLC-PD-DIM) control multiple fixtures being fed from multiple circuits?

Replacement parts for iLumin Plus?

How do I connect multiple OAC-DT-2000 motion sensors?

I am looking for a wiring diagram for Novitas 13-031 Switchpack

I'm looking for information on Novitas super switch mini model 01-220

OAC-DT Troubleshooting: Lights Will Not Turn OFF Automatically

How can I put the Room Controller into occupancy mode (auto on)?

I am looking for a single pole lighted switch?

Where can I get a manual for the SwitchKeeper lighting control panel?

Where can I get the manual for Keeper Enterprise V8.02?

How many low voltage motion sensors can be wired to an SP20-MV switchpack?

What are the installation instructions for the OS310U?

Is there a diagram for a GMDS switch connected to an occupancy sensor?

Is the OCC-RJ45 coupler included with the OACDT1000 sensor?

Looking for a wiring diagram for a NOVITAS HEAVY DUTY SWITCH PACK # 13-051

I need a Novitas 01-300-BAS two way dual tech occupancy sensor.

how do i use the remote so i could program the switch

Why is the daylight sensor (DSRC-FMOIR) for the Room Controller not dimming the lights?

How do I correct the red flashing data light on the GDS-I ?

Looking for an equal of Novitas part number 13-031.

I have wired 3 sensors to a room controller, everything is working but I noticed the limitation is 2. Would this eventually cause the sensors to fail?

Where can I get a programming guide for iCANSOFT?

Where can I find a generic lighting control specification?

LK 4/8 Greengate Digital Switch (GDS) Programming

I am looking for cut sheet on CK4-SLRC

What is Fifth Light LMS?

How do I wire a motion sensor to the UIG?

Can you overide the daylight sensor on a room controller?

What is the catalog number for a ControlKeeper4A transformer ?

Can a PIR motion sensor detect through glass?

Lights wired to Room Controller turn ON but remain at a dimmed level (lighting does not respond to dimming raise controls). How do I troubleshoot?

Where can I get Keeper Enterprise software version 6.02?

How do I get my OAC-DT-2000-DMV to turn the lights out?

What is a DAC

With the OAC-DT-2000-R motion sensor, can I install 0-10v dimming on this sensor , so the daylight sensor option dims the lights?

Can I use a DLC-PD-DIM photocell with a SF10P dimmer?

How do I program the AV scene for the RC3D?

How does the Relay interface Module work?

How do you use the HHPR-RC personal remote with the room controller?

How much current can a DLC-PD-DIM sink on the 0-10V side ?

Where can I find a wiring diagram for Greengate motion sensors with switchpacks?

How do I find a manual for a novitas 01-190 occupancy sensor

Basic Contact Closure Switch Setup step 3

I need to reset the OS310U motion sensor.

Is there a distance restriction for 0-10v wiring?

How can I connect more than 1 switchpack to the Room Controller ?

How can I get the Room Controller's 3 dimming zones to dim independantly ?

What color is the OAC-DT-2000-R Occupancy Sensor ?

How do I wire a GDS switch to a CKT panel?

How do I program a Room Controller photocell?

What is control board part# 1180909C?

Is there an install manual for a PPS-4 sensor?

Can the SP20-mv switchpack be installed in an electrical box?

What is bathroom mode on a sensor?

Is the Ilumin Source Controller a forward or reverse phase dimming panel?

Do you have mechanically held lighting contactors?

With an older PCI ControlKeeper version 3 panel can greengate digital switches be installed on it?

Can the iLumin Source Controller (SC-UN) perform reverse phase dimming?

On the OSW-P-0451-MV can you have a manual off?

What is the maximum time a motion sensor can keep the lights on after the a person leaves the covered space?

Can I wire a ceiling sensor to an existing single pole switch?

How many switchpacks (SP20-MV) can be controlled by one motion sensor?

Does iLumin revert to full 100% light output when the LRM puts it into emergency mode?

LK 4/8 Contact Closure Switch Programming

Do the Scene Wallstations need to be configured right out of the box?

How can I connect more than one Receptacle Control Switchpack to a Room Controller?

What low voltage switch is recommended for use with Greengate lighting control panels and occupancy sensors?

Is there a video showing how to install a RC3D Room Controller ?

What does a flashing green LED mean on a OAC-DT sensor?

Where can I get detailed information regarding the Fifth Light system?

Where can I find Room Controller installation guides?

Is there a lists of verified ballasts for use with the Fifthlight system?

How do I wire line voltage to a Room Controller?

How do I wire the GDS stations to the LiteKeeper 16?

Is the MicroSet Dual Teck Line Voltage ceiling sensor compatible with LED lighting?

Do we need a OCC-RJ45 connector for a DSRC-FMOIR when there isn't any other sensor?

Do you have a patient care lighting control system?

Is there a field installable part number for the Greengate OEFP2MHOMVS Sensor?

Can I network Room Controllers with a CK2?

We had a RC3DE Room Controller delivered without the 0-10 Volt Terminal Adapters. When we received the new terminal adapters, they came with capacitor and 0-10V Leads attached. What is the purpose f

I am looking for a product overview of the Greengate room control system.

What is the Lighting Sweep option on an OAC-DT sensor?

Can you program scene 6 on a RC3 room controller?

Does the daylight sensor affect all three zones in the room controller?

How do you adjust a PPS-5 sensor?

What can you do with the Ethernet port in the iLumin cabinet?

What is the part number for a ControlKeeper Touchscreen Logic Board?

Where can I get instructions for replacing a power (output) card in an SC-UN-FT?

I need optical fiber plugin for dialux software .

Where can I get SPOC installation instructions?

Which architectural dimmers are led compatible 120v residential low voltage recessed lighting

How to I connect the PPS5 sensor?

With a TSW-MV, Can a 4-way switch be used for rooms which have 3 entrances with switching of the lighting?