Eaton Logo

Greengate

What is the difference between a vacancy sensor and an occupancy sensor ?

What is the phone number for Cooper Controls ?

What is walk-through mode on a sensor?

How do I connect multiple OAC-DT-2000 motion sensors?

How many LED lights can I control with the SF10P dimmer?

WHAT IS THE DIFFERENCE BETWEEN THESE? WBSD-DEC-C1 AND WBSD-010DEC-C1

Is there a diagram for a GMDS switch connected to an occupancy sensor?

I am looking for OSP20-RDH

Can I use the CEPC-1-D with the LiteKeeper panels?

Where can I find information on the Keeper Enterprise software ?

With the OAC-DT-2000-R motion sensor, can I install 0-10v dimming on this sensor , so the daylight sensor option dims the lights?

Where can I find information on the OCC-RJ45 input/output device?

Can the Photodiode Sensor (DLC-PD-DIM) control multiple fixtures being fed from multiple circuits?

Where can I get a manual for the SwitchKeeper lighting control panel?

Where can I get the manual for Keeper Enterprise V8.02?

Why is the daylight sensor (DSRC-FMOIR) for the Room Controller not dimming the lights?

What cable do I use for wiring GDS stations?

Can I get a Novitas 01-400?

How do I wire a GDS switch to a CKT panel?

Is the OCC-RJ45 coupler included with the OACDT1000 sensor?

What is the position of the termination jumper on a GDS-I-KIT for on and off?

Is there a distance restriction for 0-10v wiring?

How do I program a Room Controller photocell?

Please advise cross for Novitas 13-031

I'm trying to replace a Novitas model 01-DL401.

How do you wire a PPS-5 to a Greengate panel?

Where can I find information on the OMC-U-2000 Occupancy Sensor ?

How can I wire more than two motion sensors to a Room Controller?

What is the part number for a ControlKeeper Standard Relay Card ?

What cable type is used to network Greengate Panels ?

Where can I find manual/documentation for the LiteKeeper 16/32?

How do I wire and adjust Demand Response on the Room Controller?

How much current can a DLC-PD-DIM sink on the 0-10V side ?

Where can I find information on the ControlKeeper 4A (CK4A) panel?

Can you use the HHPRG-RC for more than 1 Room Controller, or do I need one per RC System?

Can I connect a pps-4 to a controlkeeper to control multiple relays using programming?

Lights wired to Room Controller turn ON but remain at a dimmed level (lighting does not respond to dimming raise controls). How do I troubleshoot?

How do you Set the COM Port for Serial Communications in a LiteKeeper panel ?

I am looking for cut sheet on CK4-SLRC

What voltage does the skylight control option output on the Room Controller ?

Does the NeoSwitch integrate daylighting and occupancy sensor combination?

Can I use Timeclock mode and motion sensors with a Room Controller ?

Where can I find information on a OMC-P-1200-R Occupancy Sensor ?

Where can I find information on the Receptacle Rated Switchpack, SPRC-R-20-120, SP-R-20-120 ?

Where can I find information on the Dual Relay Switchpack, SPD20-MV-NO ?

How do I override the schedules or switches of my LiteKeeper or ControlKeeper panel ?

What are the installation instructions for the ONW-D NeoSwitch?

Do we need a OCC-RJ45 connector for a DSRC-FMOIR when there isn't any other sensor?

I have wired 3 sensors to a room controller, everything is working but I noticed the limitation is 2. Would this eventually cause the sensors to fail?

Can you overide the daylight sensor on a room controller?

Can I get a programming guide for a CK4A panel?

Can I get a user guide for a CKT panel?

How do you put the ODC-U-2000-25-R into test mode?

Can the SP20-mv switchpack be installed in an electrical box?

How do you use the HHPR-RC personal remote with the room controller?

How do you adjust a PPS-5 sensor?

Can the PPS-5 photosensor be used with any Greengate panel?

With an older PCI ControlKeeper version 3 panel can greengate digital switches be installed on it?

I need information about the dip switches on the OSW-P-0451

How do I troubleshoot a LiteKeeper 16 or 32 transformer?

What low voltage switch is recommended for use with Greengate lighting control panels and occupancy sensors?

Is the DSRC-FMOIR (Room Controller Daylight Sensor) an open loop or closed loop daylight sensor?

How can I get the Room Controller's 3 dimming zones to dim independantly ?

What is in a RC3D Room Controller QuicKit ?

Where can I get Keeper Enterprise software version 6.02?

Where do I find instructions or tutorials for the LiteKeeper 4 & 8?

Do you have a 0-10v photocell

Where can I find information on the Extreme Temperature Sensor, OXC-P-1500-R, OXC-P-2MH0-R ?

Where can I find information on the Digital Wall Switch Timer, TSW-MV-W ?

Where can I find information on a Momentary Decorator Switch ?

Where can I find information on the ControlKeeper MB, CKMB panel ?

Where can I find information on the PD216 Power Dimmer ?

What 3 wire momentary switch is offered for use with Greengate lighting control panels?

How many low voltage motion sensors can be wired to an SP20-MV switchpack?

Can I use Keeper Enterprise for LiteKeeper panels ?

How do I wire line voltage to a Room Controller?

How do I program switches with a LiteKeeper 8?

Can a dimming command be broadcasted from a CKT to a CK4A?

Looking for an equal of Novitas part number 13-031.

Can I use a DLC-PD-DIM photocell with a SF10P dimmer?

Can I get a user guide for a LK16/32 LiteKeeper panel?

What are the causes of a CKT panel touch screen indicating that it cannot see the relays in the panel?

How does the daylighting feature work on a NeoSwitch wall switch sensor?

Can you use vacancy sensors with the RC3D Room Controller ?

What is the catalog / part number for a ControlKeeper Touchscreen Transformer ?

Where can I get installation instructions for the WEIM?

Is the OEC-U-1001 a discontinued item? If so what model should i use instead?

Can more than one daylight sensor (DSRC-FMOIR) be used with one Room Controller?

Can more than one Greengate motion sensor be used with the SP20 when using a low voltage switch for manual control?

What is the maximum length of Cat 5 cable connected to a Room Controller device?

Where can I find the user manual / installation guide for a Novitas 1-400R PIR switch?

How do I create a switch timer on a CKT panel ?

If we order a four button GDS switch with blank buttons can we change them out once the customer engraving is completed? If so what is the process of changing out the buttons once installed in the wal

multiple rc-5tsb

How do I troubleshoot a ControlKeeper 2 or ControlKeeper 4 transformer?

Lights wired to Room Controller turn ON but remain at a full bright level (lighting does not respond to dimming lower controls). How do I troubleshoot?

How do I troubleshoot a LiteKeeper 4 transformer?

How do you program a remote command in a LiteKeeper panel ?

how do i use the remote so i could program the switch

How can I control multiple voltages with the Room Controller?