Eaton Logo

Ilumin

What is the phone number for Cooper Controls ?

Is the NS3-C sensor open loop or closed loop?

Is the Ilumin Source Controller a forward or reverse phase dimming panel?

What can you do with the Ethernet port in the iLumin cabinet?

What is replacement stem for H1319P?

What is control board part# 1180909C?

What is the part number for the Main power supply in the SC-RP Ilumin panel?

How long will iLumen panels hold programming after losing power?

Where can I find information on the iLumin iCANview-SC (ICANview Remote Scene Control Software)?

Where can I find information on the iLumin SC-UN-FT (Universal Source Controller, Feed Through)?

Are the relays in the Ilumin panel replaceable?

What is the LCNJ ?

What do the LED's do on the Ilumin HF Card?

Where can I get instructions for replacing a power (output) card in an SC-UN?

Does iLumin revert to full 100% light output when the LRM puts it into emergency mode?

Where can I find information on the iLumin Recessed Combination Sensor (NS3-C)?

Where can I find information on the iLumin SW-2 (iCANnet to PC Interface)?

How can I enable or disable an output to be affected by raise/lower commands from a wallstation or touchscreen in an iLumin panel?

Why is my iLumin panel not powering up?

How do I wire a motion sensor to the UIG?

What type of circuit breakers does the Ilumin Source Controller have?

Where can I find the CIM install manual

What size wire is recommended for use on the UIG-2-NA connections ?

How many IRTR's can be connected to the UIG-2-NA?

How should the low voltage wiring enter the Ilumin panel?

Does the CIM BAC require an IP address?

What is the part number for the Network and Accessory Power Supply for the SC-RP Ilumin panel?

Does the Ilumin panel have contact closure terminals?

Where do you land the low voltage wires in an Ilumin panel?

What size breakers are used in the Ilumin Source Controller?

Where is the Networks Power Supply Unit in the Ilumin panel?

Where can I get a programming guide for iCANSOFT?

Where can I get instructions for replacing a power (output) card in an SC-UN-FT?

Can iLumin SC-UN panels dim reverse phase fixtures?

Can an iLumin Source Controller be mounted sideways?

Can the iLumin Source Controller (SC-UN) perform reverse phase dimming?

Can I program the Dry Contact closures for an Ilumin panel using the ICanSoft software ?

Where can I find information on the iLumin EG2-NA (Ethernet Gateway)?

Where can I find information on the iLumin UIG-2-NA (Universal Interface)?

Where can I find information on the iLumin SI-2-NA (System Integrator)?

Where can I find information on the iLumin RI-2-NA (Relay Interface)?

Where can I find information on the iLumin BN-2-NA (Network Bridge)?

Where can I find information on the iLumin SCD96-NA (DMX Output Interface)?

Where can I find information on the iLumin CIM (Communications Interface Module)?

Where can I find information on the iLumin CLV Revio wallstation?

Where can I find information on the iLumin CLS Ineo wallstation?

Where can I find information on the ArchiDMX?

Where can I find information on the iLumin TSC50 (5.7” LCD color touchscreen)?

Where can I find information on the iLumin TSC30 (3.5” LCD color touchscreen)?

Where can I find information on the LRM (Lighting Relay Module)?

Where can I find information on the iLumin mobile application?

Where can I find information on the iLumin LCNJ (Lighting Control Network Jack)?

Where can I find information on the iLumin IRTR (Infrared Transmitter and Receiver)?

Where can I find information on the iLumin HH17IR infrared handset?

Where can I find information on the EXPS-15V (External Power Supply)?

Where can I find information on the iLumin SC-UN (Universal Source Controller)?

Where can I find information on the iLumin SC-RP (Switched Relay Controller)?

Where can I find information on the iLumin SC-RPB (Switched Relay Controller with Circuit Breakers)?

Can I use cat6 cable to control a Universal Source Controller?

Can I use cat5e cable to control a Universal Source Controller?

Why does my new Outputs Power Supply have 6 terminal screws while my old one has 4 ?

Is there an iLumin panel capable of mixed load voltages?

What is the maximum load for the SC-UN (Universal Source Controller) panel?

Can the SC-UN panel be fed from the bottom?

How do I re-number a power card in an iLumin SC-UN?

Can I order a 3 phase iLumin SC-RP?

How can I change my iLumin touchscreen logo?

How can I get documentation and software for the ADMX control device?