Eaton Logo

Can I program the Dry Contact closures for an Ilumin panel using the ICanSoft software ?

Yes, in addition to using the onboard interface of the Ilumin panel, you can use ICanSoft to program the dry contact closures. Just open IcanSoft and then open the Inputs tab. Click on the Edit box next to the input number and a window will popup that allows you to configure the input close/open options.