Eaton Logo

Where do you land the low voltage wires in an Ilumin panel?

Low voltage wiring terminates on the channels of the HF Card. Terminal blocks are removable for ease of wiring. The HF Card automatically senses whether it needs to be a sink or source for the 10V supply. If it is sourcing the 10V, it can source approximately 20mA per HF Channel.