Eaton Logo

Occ Sensors

What is the difference between a vacancy sensor and an occupancy sensor ?

What is walk-through mode on a sensor?

Can I block a PIR motion sensor’s view?

Can a PIR motion sensor detect through glass?

Looking for an equal of Novitas part number 13-031.

Can I get a Novitas 01-400?

How do I connect multiple OAC-DT-2000 motion sensors?

What type wire should be used to connect to Greengate Motion sensors?

How do I get my OAC-DT-2000-DMV to turn the lights out?

Please advise cross for Novitas 13-031

How does the daylighting feature work on a NeoSwitch wall switch sensor?

Where can I find information on the iLumin Recessed Combination Sensor (NS3-C)?

With the OAC-DT-2000-R motion sensor, can I install 0-10v dimming on this sensor , so the daylight sensor option dims the lights?

Where can I find a wiring diagram for Greengate motion sensors with switchpacks?

What does a flashing red LED mean on a OAC-P sensor?

What does a flashing green LED mean on a OAC-DT sensor?

Can I use multiple OAC -R occupancy sensors with only one SP20-MV when using the daylight sensor function?

I would like to find information about the OAC-U-1000-R

Where can I find information on MicroSet Passive Infrared Low Voltage Occupancy Sensing Ceiling Sensor OAC-P-0500-R, OAC-P-0500, OAC-P-1500-R, OAC-P-1500 ?

Is the OEC-U-1001 a discontinued item? If so what model should i use instead?

Can a photocell be wired to a sensor?

Can I wire a ceiling sensor to existing three-way switches?

What is ultrasonic technology for motion sensors?

What is the maximum height a ceiling mounted motion sensor can be installed?

How do I make my OAC-DT-2000 less sensitive ?

Where can I find information on the MicroSet PIR Line Voltage Occupancy Sensing Ceiling Sensor OAC-P-0500-MV, OAC-P-0500-DMV, OAC-P-1500-MV, OAC-P-1500-DMV ?

Can the motion sensor for the Metalux SNLED be field installed? 2SNLED? 4SNLED? 8TSNLED?

How do I place the OAC-DT-1000 sensor into test mode?

What is bathroom mode on a sensor?

Can I control both 120VAC and 277VAC with one ceiling mounted motion sensor?

Can I use a ceiling mounted motion sensor in a shower room?

What is the maximum time a motion sensor can keep the lights on after the a person leaves the covered space?

Can I set a wall switch sensor to work as a regular ON/OFF switch?

Can I connect a sensor to an EMS(BMS) system?

28. Can I use a dual relay wall switch sensor in a single load application?

Can I wire a ceiling sensor to existing three-way switches?

What is PIR (Passive Infrared) Technology for motion sensors?

Does an Ultrasonic Motion Sensor detect audible noise?

What is the maximum wire distance between motion sensors and switchpacks (SP20-MV)?

How many switchpacks (SP20-MV) can be controlled by one motion sensor?

Is it possible to wire an OAC-DT line voltage ceiling sensor in parallel with another OAC-DT sensor? If so, is there a limit to the number of parallel devices? Thanks

What color is the OAC-DT-1000-R Occupancy Sensor ?

Can I wire an OAC-DT-2000-MV to an SP20-MV?

Can I run OAC motion sensors in parallel on the same channel of a Greengate lighting control panel?

Is the OAC-P motion sensor rated for outdoor use?

Can I use a ceiling mounted motion sensor in an outdoor application?

Can a wall switch sensor control both a light fixture(s) and an exhaust fan?

What color is the OAC-DT-2000 Occupancy Sensor ?

Can the SP20-mv switchpack be installed in an electrical box?

How does the energy saver mode work on the OMC-DT-2000-R sensor?

Where can I find the user manual / installation guide for a Novitas 1-400R PIR switch?

What is the minimum time delay for a motion sensor?

How far from an air ducts (vents) should I install motion sensors?

Do sensors have integrated photocell?

Do sensors have integrated relays?

Do sensors affect fluorescent lamp life?

Can I wire a ceiling sensor to an existing single pole switch?

Can I wire a ceiling sensor to an existing single pole switch?

In regards to motion sensors, what is the NEMA WD7 Standard?

In regards to motion sensors, what is major motion?

In regards to motion sensors, what is minor motion?

What is a dual technology (DT) motion sensor?

Does a PIR sensor detect a person’s body heat when they're not moving?

What ultrasonic frequencies are used in motion sensors?

Can I block an Ultrasonic motion sensor’s view?

Can an Ultrasonic Motion Sensor detect through glass?

What do the motion sensor LEDs indicate?

What size wire is recommended to use between motion sensors and switchpacks (SP20-MV)?

What does a flashing red LED mean on a OAC-DT sensor?

What color is the OAC-DT-2000-R Occupancy Sensor ?

What color is the OAC-DT-1000 Occupancy Sensor ?

Where can I find information on the MicroSet Ultrasonic Low Voltage Occupancy Sensing Ceiling Sensor,OAC-U-2000-R, OAC-U-2000, OAC-U-1000-R, OAC-U-1000, OAC-U-0501-R, OAC-U-0501?

Where can I find information on MicroSet Ultrasonic Line Voltage Occupancy Sensing Ceiling Sensor OAC-U-2000-MV, OAC-U-2000-DMV ?

Where can I find information on the MicroSet Dual Tech Line Voltage Occupancy Ceiling Sensor, OAC-DT-2000-MV, OAC-DT-2000-DMV ?

Where can I find information on MicroSet Dual Tech Low Voltage Ceiling Sensors OAC-DT-2000-R, OAC-DT-2000, OAC-DT-1000-R, OAC-DT-1000, OAC-DT-0501-R, OAC-DT-0501 ?