Eaton Logo

OAC-DT Motion Sensor Troubleshooting

To place the sensor into Test Mode, toggle DIP Switch 10 out of its current position, wait 3 seconds, and then back into its original position. To force into 10 min User Mode move Dip Switches 1 and 2 down. (If DIP Switches 1 and 2 are already down, toggle DIP Switch 1 out of its current position, wait 3 seconds, and then back to its original position) While in Test Mode, the LEDs will flash once per 1/4 second.
 
1. Walk around the room and monitor LEDs. LEDs should only turn ON for ¼ second with each motion.
2. Stand still six to eight feet away from the sensor for five seconds. LEDs should not turn ON.
3. Walk outside the room and wait 15 seconds for the lights to turn OFF.
4. Re-enter the room to activate sensor.
5. The unit will remain in Test Mode for 10 minutes then automatically exit Test Mode and go to 10 min. Time Delay User Mode setting.
 
If the sensor does not operate properly, then select from the choices below to continue troubleshooting.